AXIS#.MOTOR.VRATED

Description

This parameter configures the drive for the rated velocity of the induction motor as indicated on the nameplate. AXIS#.MOTOR.VRATED is used to calculate the constant volts per Hertz characteristics of the drive and motor.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 2.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

1200 RPM

Depends on units. See Velocity Units for details.

Data Type

Float
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
AXIS1.MOTOR.VRATED

500bh

0bh

Signed32

Velocity

-

Read/Write

No

AXIS2.MOTOR.VRATED

510bh

0bh

Signed32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.VRATED

6227

1853

Signed32

Read/Write

Velocity

AXIS2.MOTOR.VRATED

71763

1185

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.VRATED

6227

Float

Read/Write

Velocity